ADC ISR problem on MPC5604B using CW for MPC55xx and MPC56xx 2.9

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

ADC ISR problem on MPC5604B using CW for MPC55xx and MPC56xx 2.9

1,155件の閲覧回数
earendil
Contributor I

Hi!

 

I've been stuck for several days and simply cannot solve the problem.

Here is initialization of ADC.

 

void initADC(void) {ADC.MCR.R = 0x00000000; /* Initialize ADC one shot mode*/ADC.NCMR[0].R = 0x00000007; /* Select ANP1:2 inputs for normal conversion */ADC.CTR[0].R = 0x00008606; /* Conversion times for 32MHz ADClock */}

 init of interrupt

 

//initialization of interruptvoid init_ADC_int(void){ADC.IMR.B.MSKEOC = 1; /*Interrupt Mask bit End Of Conversion*/ ADC.CIMR[0].B.CIM0 = 1; /*Channel Interrupt Mask bit*/}

 and in the main I call functions above plus

INTC_InstallINTCInterruptHandler(ADC_vect, 62, 1);

 in forever loop I start single conversion

if(BUTTON2_PRESSED)// button 2 pressed receive command { ADC.MCR.B.NSTART=1;       /* Trigger normal conversions for ADC0 */ while (ADC.MSR.B.NSTART == 1) {};}

 However interrupt routine never performs

 

When I put this piece of code in main loop it works, but it's not an interrupt

if(ADC.ISR.B.EOC==1) /*Check for End Of Conversion Flag */ ADC_vect();/*ADC interrupt routine*/

 

Please point me to the right direction I have spent so much time and need to get this working.

 

And the last thing, from example it says:

ADC.NCMR[0].R = 0x00000007;

But how can I write 0x7; ->bit 0,1 and 2 to register(seems it's accessible from bit 16-31). If I want CH0 CH1 CH2 shouldn't I rather set  bit 31, 30 and 29 according to bit table in 'MPC5604B/C Microcontroller Reference Manual' page 760? And thus

ADC.NCMR[0].R = 0xE0000000;

 

Thanks for reply

ラベル(1)
タグ(1)
0 件の賞賛
3 返答(返信)

513件の閲覧回数
stanish
NXP Employee
NXP Employee

Hi earendil,

 

Have you enabled the external interrupts properly?

 

INTC.CPR.B.PRI = 0; /* Single Core: Lower INTC's current priority */asm(" wrteei 1");   /* Enable external interrupts */

 Stanish

0 件の賞賛

513件の閲覧回数
earendil
Contributor I

Hi Stanish,

 

I'm using function from example:

void enableIrq(void) { INTC.CPR.B.PRI = 0;          /* Single Core: Lower INTC's current priority */ asm(" wrteei 1");         /* Enable external interrupts */}

 Anyway, PIT interrupt and external interrupt work.

 

earendil

0 件の賞賛

513件の閲覧回数
rk1
Contributor I

I am trying something similar with CTU connection. I face the same problem. Conversion is done but not getting interrupts.

I have configured interrupts for emios channels and they are working.

let me know if you found a solution for this problem

 

Ravi

0 件の賞賛