U-Boot Debug using CodeWarrior for QorIQ LS series – ARM V7 ISA
Hi,
I have a problem on loading u-boot into our bareboard.
I have a customized LS1021A bareboard, how could I load u-boot into this board?
I compiled a u-boot and tried to attach it by a CodeWarrior TAP, but I always got some JTAG configuration failure.
Error launching LS1021AQDS_Debug_LS1021AQDS_Attach
CCSProtocolPlugin : Failed to correctly configure the JTAG chain
Is an on-board programmed u-boot necessary? Or I should change the target initialization file too?
Thanks
Hi Adrian,
I'm working on a custom board now. I have made a working u-boot for my board.
But still I cannot debug the file "u-boot" normally,
While I reset it(Figure 10), what I get is different from Figure 11, there is no place to set the source code location.
Here is the message:
No source available for "0x00001EC0 (0x00001EC0)() "
I just try on my QDS board and after reset without init, CW will prompt for source location. Could you please file on u-boot elf and provide the results.
My u-boot elf for nand boot looks like below:
$ file u-boot
u-boot: ELF 32-bit LSB shared object, ARM, version 1 (SYSV), dynamically linked (uses shared libs), not stripped
Hi Adrian,
My file information is the same, but while I reset without any init file, here is what's inside the debug window:
100 of_read_number() fdt_support.c:1397 0x00000000
99 of_read_number() fdt_support.c:1397 0x00000000
98 of_read_number() fdt_support.c:1397 0x00000000
...
3 of_read_number() fdt_support.c:1397 0x00000000
2 of_read_number() fdt_support.c:1397 0x00000000
1 of_read_number() fdt_support.c:1397 0x00000000
If I press "Step Over"/ "Step Into", it will prompt
No source available for "0x00001EC0 (0x00001EC0)() "
If I choose Resume/Step Return, it won't prompt anything and I can only Pause or Terminate it.
Besides, I have tried to debug linux kernel and it didn't prompt for source location either.
I delete the whole workspace and redo those steps, but it doesn't work.