i have purchased two DEMO9S08DZ60 board out of them one providding error related to trriming issue and when i try to load programme in it it gives third party downloaded software error i sended that error report to freescale through your software code warrier but still issue is there i checked same hardware in different computer same issue is there another one is working properly so what i do
Solved! Go to Solution.
from the error message, "bad argument pass to function", it is related with code. can you please upload your project here?
Have a great day,
Zhang Jun
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
hello
this is a connection problem, we need to check both board and SW.
1. board:
connect the board with computer, take a photo of it and upload the photo here, i need to check the board jumper setting.
2. PC SW:
CW10.2 is too old, please use CW10.6.4
CodeWarrior for Microcontrollers-Eclipse IDE|Freescale
to avoid old associations, pls
a) create a new workspace,
b) create a new project with wizard and test this new project in this new workspace.
let me know how it works?
Have a great day,
Zhang Jun
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
this way message comes and afterward try retry button multiple time but it not work .
can you send us the photo the the problemable board while connecting computer?
did you ever try use external power supply to test it?
did you try create a new project to test it?
how it works if you use external emulator, for instance BDM Multilink?
Have a great day,
Zhang Jun
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
hello sir/madam,
i never tried external power supply i apply through USB cable from laptop
and used PE multilink internal debugger of codeworrier.i tried new
workspace and new project eventhough there is same problem
some time it gives error related to trimming also
here i am attaching board photo and error screenshot please refer it,
thanks and regards,
hitesh lad
On Fri, Aug 21, 2015 at 4:52 PM, ZhangJennie <admin@community.freescale.com>
HI,
i checked your demo-dz60.jpg. the jumper setting and led status are correct.
from the log information, the flash module was not erased successfully.
I wonder the problem is on board side. I am not sure if your board/MCU is in good condition.
can you please use same computer/same cable/same project to test your other board. if if the problem is only in one board, I wonder the board or MCU is corrupt. Please use BDM port and external BDM multilink to test the board. thus we can know the corrupt part is on on-board emulator or MCU.
Have a great day,
Zhang Jun
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
from the error message, "bad argument pass to function", it is related with code. can you please upload your project here?
Have a great day,
Zhang Jun
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
dear sir/madam,
thank you very much fro your support can guide me how i can use BDM port ?
i only used USB cable port? what other requirements are ther? powersupply
or cables?
thanks and regards,
hitesh lad
On Tue, Aug 25, 2015 at 2:11 PM, ZhangJennie <admin@community.freescale.com>
Hi
refer the steps listed :
http://cache.freescale.com/files/microcontrollers/doc/user_guide/DEMO9S08DZ60_UG.pdf
page7, Debug Mode
Debug mode is available to the user through the integrated USB-Multilink BDM or through the use of an external HCS12/HCS08 BDM cable. Use of the integrated USB-Multilink BDM requires only a host PC with an available USB port and an A/B type USB cable. A 6-pin BDM interface header(BDM_PORT) supports the use of an external HCS12 BDM cable. The BDM_PORT header is not installed in default configuration.
here is the link for USB-Multilink BDM
www.freescale.com/webapp/sps/site/prod_summary.jsp?code=USBMULTILINKBDM
Have a great day,
Zhang Jun
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
sir i order two module at a same time one is working with 10.2 another have problem when we load it move up to 76% then simply show third party software down load and not moving in debugging mode
please test if the same project under same CW, work for one board but can't for another. the problem may be on board side.
did you do this test?
Have a great day,
Zhang Jun
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi Hitesh,
Could you tell us which CodeWarrior version are you using? Also could you post an screenshot of the error?
Thanks in advance!
Best Regards,
Carlos Mendoza
Technical Support Engineer
sir i have same kind of onotherboard which is functioningproperly only one board have issue so i dont think code warrior version isssue is there
i use codewarrior-10.2