Which is the best version Of CODE WARRIOR to compile micocontroller MC9S12A128?
Link Order View
The Link Order view of the Project window shows information about
how the IDE will compile or link the final output file for the project's current build
target.
The IDE links the files in order from top to bottom. For example, if file B depends on
file A, make sure that the Link Order view lists file B below file A.
what it means?
Hi
In order to separate different type of questions, I suggest you create new thread for the new question.
Thanks!
Jennie
Is only main.c added in souce directory of code warrior?
if you create a project with wizard, you will see besides main.c, there are also other .c, .h. .prm files. see it
Have a great day,
Jennie Zhang
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
If i create different *.c files like RS232.c , spi.c etc. is it necessary to add this to souce directory?
LIKE THIS
the created files are customized files. Whether adding them to the project depends on customer side. I don't know what are those files for and what's inside.
For CW itself, it supports adding multi- files for build.
Hi.
Please use CW5.1. Attached is the video of how to download CW5.1.
Have a great day,
Jennie Zhang
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Is MC9S12A128 and MC9S12A128B are same?
you can use 9s12A128B for 9s12A128 in CW5.x.
But Please know that the MC9S12A128B and the MC9S12A128 are not completely qualified,
they are pin compatible, however not necessarily code compatible depending on their errata work around,
which you can find on the link listed below:
Have a great day,
Jennie Zhang
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------