Under CodeWarrior for MCUs v10.2:
1) Choose Project > Properties.
A Properties for Project xxx window appears.
2) Choose C/C++ Build > Settings
The Settings view appears.
3) Choose ARM LInker > Input, then check Suppress Link Warnings.
---Tom
Tom,
Thanks. I had guessed that much, but found nothing. After reading your reply, I still found nothing; but I decided to dig deeper. My apologies for not saying I'm using CodeWarrior 6.1, which I'm sure has different menus. This is what I found:
Edit > Standard Settings...
"Target Settings Panels" Target > Linker for HC08
"Command Line Arguments" Box [Here is where I assume I could add "-WmsgSd1107".]
But, I decided to create a new project with different settings, and this "Warning" no longer appears
Thanks,
-Mike
That is correct. The Command Line Options box is where you would enter the argument. You can also click on the Messages button which displays a panel where you can enable/disable/warn various messages. When you are done with this panel, click OK and the IDE automatically generates the proper arguments and inserts them into the Command Line Options box.
---Tom