When is Freescale going to release a OSBDM dll that will...

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

When is Freescale going to release a OSBDM dll that will...

跳至解决方案
2,014 次查看
UcTechnoGeek
Contributor II
When is Freescale going to release a OSBDM dll that will support the MCF51 Flexis family???

I know the built-in debugger is based on the 9S08 debugger, so the OSBDM hardware should work with the the Flexis coldfire parts.

Are they just trying to protect the margins of the over-priced third party tools or have they given up on the small customers and hobbyist by only offering 1/2 support?

Regards,
Frustrated uCTechnoGeek
标签 (1)
标记 (1)
0 项奖励
1 解答
490 次查看
osbdm_support
Contributor II
Hello all, I have been recently assigned to support OSBDM on the forums.   We are still having some internal discussion relating to OSBDM, and we are waiting on posting anything to the forums till the discussion is complete.  Please be patient.

Thanks!

Dan Leech
osbdm-support@freescale.com

在原帖中查看解决方案

0 项奖励
3 回复数
491 次查看
osbdm_support
Contributor II
Hello all, I have been recently assigned to support OSBDM on the forums.   We are still having some internal discussion relating to OSBDM, and we are waiting on posting anything to the forums till the discussion is complete.  Please be patient.

Thanks!

Dan Leech
osbdm-support@freescale.com
0 项奖励
490 次查看
UcTechnoGeek
Contributor II
My appologies to Freescale.

The new CW version 6.2 that was just released does support the OSBDM connection.

Now, we just need to make it work with the OSBDM connection.

uCTechnoGeek
0 项奖励
490 次查看
J2MEJediMaster
Specialist I
FWIW, we do have a person recently assigned to handle OSBDM support. I've forwarded this forum thread to him. He's plenty busy, so I can't vouch for when he might get to this. But he has been made aware of the issue.

---Tom

0 项奖励