USB-ML-12 for target MC9S12XDP in CodeWarrior 4.5 or 4.6?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

USB-ML-12 for target MC9S12XDP in CodeWarrior 4.5 or 4.6?

ソリューションへジャンプ
2,433件の閲覧回数
Pang
Contributor I
Hi everyone,
 
Recently, I just purchased USB-ML-12 from P&E Micro. I am going to use it as a connection for debugging  in CodeWarrior V4.5/V4.6. I just install the drive for USB-ML-12. When I created a new project in Page 10,
 
I chose P&E MultiLink/Cyclone for connection. Do I still need to install any other debugger utilities from P&E Micro so that I can debug for my target MC9S12XDP in CodeWarrior?
 
Thanks,
 
Pang
 
 
 
ラベル(1)
タグ(1)
0 件の賞賛
返信
1 解決策
946件の閲覧回数
J2MEJediMaster
Specialist I
You should be about ready. Try running the debugger (Project | Debug) and see if True-Time Simulator and Real-Time Debugger launches.

---Tom

元の投稿で解決策を見る

0 件の賞賛
返信
3 返答(返信)
947件の閲覧回数
J2MEJediMaster
Specialist I
You should be about ready. Try running the debugger (Project | Debug) and see if True-Time Simulator and Real-Time Debugger launches.

---Tom
0 件の賞賛
返信
946件の閲覧回数
Pang
Contributor I
I just tried and it was working!!!. Thanks a lot, Alban and Tom.
 
Pang
0 件の賞賛
返信
946件の閲覧回数
Alban
Senior Contributor II
Hi Pang,

No, you don't need anything else.
P&E utilities are bundled with CodeWarrior as standard.

Cheers,
Alban.

Message Edited by Alban on 2007-01-25 04:05 PM