Trim the internal clock frequency of KL16 to other value in CW10.6

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Trim the internal clock frequency of KL16 to other value in CW10.6

628 Views
Roger_Fan
NXP Employee
NXP Employee

Hi, I am using KL16 with CW10.6 and JLink. Want to change the trim value of the internal clock source from default 32.768KHz to 31.25KHz. Where in CW can I make the internal clock source speed changes?

 

Thanks!

Labels (1)
0 Kudos
Reply
1 Reply

499 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi Roger.

I think this document should answer your questions:

Yes, OSDA can trim the reference of internal clock source!

can this help?


Have a great day,
Zhang Jun

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply