I have generated SWI and SYS interrupts using processor export
->In modules ->vector table ->Vsys,Vswi configured and code generated .while building code its saying functions undefined in Vswi.c file contain definition but its commented ..is their any problem to create Vswi,Vsys.
if no can pls help me to crate interrupts and code generation
Thanks
Rajesh
Hi Rajesh,
Could you tell us which MCU are you using?
Thanks in advance!
Best Regards,
Carlos Mendoza
Technical Support EngineerRajesh
Hi Rajesh,
You can enable these two interrupts in CPU properties. then generate pe code, you will see the related vector and interrupt function generated. See attached video.
Have a great day,
Jennie Zhang
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi pls find the above pics I can able create interrupts from components ...but ur suggestion in cpu component inspector is it both are same .
S12zvc have any core self test functionality check .on of the document saying having SCST module for S12ZVC.
Thanks ,
Rajesh Kota
Hi Rajesh,
I believe your last two screenshots are generated by component InterruptVector. Something like Vsys.c. Vswi.c
In CW10, these c files from InterruptVector component are commented. To use the generated functions, we need manually copy them for example
to User modules:
main.c
or
Events.c
These are also suggested under comments.
Have a great day,
Jennie Zhang
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi Jennie ,
1)My question is Both process of creating interrupts different but result is it same ?
2)Core self test component is avail for S12Zvc if its is yes can you pls give me over view of Self test module .
thanks
Rajesh Kota
Hi Rajesh Kota
Regarding to your questions:
>>1)My question is Both process of creating interrupts different but result is it same ?
Answer: Correct.
>>2)Core self test component is avail for S12Zvc if its is yes can you pls give me over view of Self test module .
Answer: I don't think we have core self test component.
Have a great day,
Jennie Zhang
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------