Regarding New Purchase to CodeWarrior.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Regarding New Purchase to CodeWarrior.

1,904 Views
PoojaKat123
Contributor I

Hello,

For MC68HC908AB32 microcontroller which CodeWarrior version is required? . what is the difference between CW IDE 6.3.2 and CW for MCU 11.1.?

 

Thanks and Regards

Pooja Katariya

0 Kudos
Reply
15 Replies

1,846 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

HI,

MC68HC908AB32 is very old product. It is only supported on CW6.3 now:

https://www.nxp.com/design/software/development-software/codewarrior-development-tools/codewarrior-l...

CW6.3 is legacy product. It works on Windows XP/Vista 32-bit , but doesn't support win7/10/11 64bit.

CW for MCU 11.1 doesn't support HC08 device. It supports HCS08.

Hope this helps,

Jun Zhang

 

0 Kudos
Reply

1,624 Views
PoojaKat123
Contributor I

Hi

for this MC68HC908AB32 , which exe file should I download, In below link here is so many file is showing.

 

https://nxp.flexnetoperations.com/control/frse/download?agree=Accept&element=5901331

 

 

0 Kudos
Reply

1,620 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

I can't open this link. Please send me a screenshot. Thanks.

0 Kudos
Reply

1,605 Views
PoojaKat123
Contributor I

Hi Zhang Jennie.

If I am installing CodeWarrior for Microcontrollers (RS08HC(S)08-ColdFire V1) v6.3.exe for MC68HC908AB32CFU In my Machine which have XP window  then this below error is coming.

The contents of this file cannot be unpacked The executable you are attempting to run has been Corrupted please obtain another copy of the file verify its integrity and try again.

Do you have any idea why this error is coming.

Thanks and Regards

Pooja Katariya

 

 

0 Kudos
Reply

1,589 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

This is an another question. To saperate different subject, please create a new thread to ask with the problem screenshot.

Thanks,

Jun Zhang

0 Kudos
Reply

1,611 Views
PoojaKat123
Contributor I

I am not able to download the link which you have shared for CodeWarrior version.

Can you please share the details which version should I download in XP Pc for MC68HC908AB32CFU.

0 Kudos
Reply

1,837 Views
PoojaKat123
Contributor I

Thanks for your revert ,

Is there any product available which is compatible with this MC68HC908AB32 product. If it is available then we can replace this product.

 

Thanks and Regards

Pooja Katariya

0 Kudos
Reply

1,829 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi PoojaKat123,

There is no pin to pin device to MC68HC908AB32. I suggest LPC80x device as replacement.

https://www.nxp.com/products/processors-and-microcontrollers/arm-microcontrollers/general-purpose-mc...

LPC80x build toolchain is MCUXpresso IDE.

Hope this will help you,

Jun Zhang

0 Kudos
Reply

1,823 Views
PoojaKat123
Contributor I

Hi,

Thanks for your response, this product series is available for 64 pin or not?

 

 

0 Kudos
Reply

1,815 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi PoojaKat123 

No. If 64pin is must, I suggest LPC845M301JBD64 or LPC844M201JBD64 

https://www.nxp.com/part/LPC845M301JBD64#/

https://www.nxp.com/part/LPC844M201JBD64#/

 

LPC845 supports DAC and cap touch, LPC844 doesn't. Other features are the same.

Hope this helps,

Jun Zhang

 

 

0 Kudos
Reply

1,731 Views
PoojaKat123
Contributor I

Hi,

Thanks for your suggestion , Which microcontroller you have suggested these have all features of MC68HC908AB32CFU, like Keyboard Interrupt , SCI transmit and receive features.

Thanks and Regards

Pooja Katariya

0 Kudos
Reply

1,711 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

The most similar part should be KE02. It also has 64k package.

https://www.nxp.com/products/processors-and-microcontrollers/arm-microcontrollers/general-purpose-mc...

Hope this helps,

Jun Zhang

0 Kudos
Reply

1,717 Views
PoojaKat123
Contributor I

Hi ,

Is there any microcontroller which is compatible with MC68HC908AB32CFU.

because these suggested microcontroller do not have all features and also do not have EEPROM , Monitor ROM.

Thanks and Regards

Pooja Katariya

0 Kudos
Reply

1,677 Views
PoojaKat123
Contributor I

Hi,

I there any microcontroller which have pin to pin connection these microcontroller not pin to pin.

 

Thanks and Regards

Pooja Katariya 

0 Kudos
Reply

1,663 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

NO, we don't have pin to pin replacement for this part.

0 Kudos
Reply