No Vpp Programming Voltage

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

No Vpp Programming Voltage

跳至解决方案
2,917 次查看
Philou
Contributor I
Hi guys
 
i'm trying to debug a S12X software, and i have this issue, no programming voltage. i have suspected a board issue. but on another one it's the same issue.
i have that on the command display:
Vppon command file correctly executed.
FP: No programming voltage
FP: No programming voltage
FP: ALL_PPAGES flash module is bad or protected.
executing .\cmd\P&E_Multilink_CyclonePro_vppoff.cmd
 
i have tried to unsecure the chip, but when i do that the debbugger crashes.
 
Any thoughts?
 
Thanks for your help.
 
Philou
标签 (1)
标记 (1)
0 项奖励
回复
1 解答
627 次查看
Philou
Contributor I
Found the issue. Even if I have checked that on the rising edge of the reset the state of MODA and MODB (low), it was not sufficient. Theses pins must be pulled down no for setting the correct MCU mode.

在原帖中查看解决方案

0 项奖励
回复
1 回复
628 次查看
Philou
Contributor I
Found the issue. Even if I have checked that on the rising edge of the reset the state of MODA and MODB (low), it was not sufficient. Theses pins must be pulled down no for setting the correct MCU mode.
0 项奖励
回复