MQX 4.2 plugin with CW 10.7

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MQX 4.2 plugin with CW 10.7

1,315件の閲覧回数
emanueletrapani
Contributor III

Hi,

i installed MQX 4.2 on my system. I use CW 10.7.

I select the mqx 4.2 plugin from CW-help-Install new software.

i followed https://community.nxp.com/thread/386551 .

When i try to install MQX 4.2 plugin i get the error:

"An error occurred while collecting items to be installed
session context was:(profile=PlatformProfile, phase=org.eclipse.equinox.internal.p2.engine.phases.Collect, operand=, action=).
No repository found containing: binary,com.freescale.coldfire.PEx_root,1.0.4
No repository found containing: binary,com.freescale.coldfire.architecture_root,1.0.7
No repository found containing: binary,com.freescale.coldfire.buildtools_root,1.0.4
No repository found containing: binary,com.freescale.hcs.PEx_root,1.0.4
No repository found containing: binary,com.freescale.hcs.architecture_root,1.0.6
No repository found containing: binary,com.freescale.kinetis.PEx_root,1.0.4
No repository found containing: binary,com.freescale.kinetis.architecture_root,1.0.7
No repository found containing: binary,com.freescale.kinetis.gcc_root,1.0.4
No repository found containing: binary,com.freescale.kinetis.segger_root,1.0.2
No repository found containing: binary,com.freescale.mqx.v4.0_root,1.4.1.201401301129"

What is my mistake?

Thank you

ラベル(1)
タグ(1)
0 件の賞賛
5 返答(返信)

932件の閲覧回数
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi Emanuele,

I would suggest you try this site :

FSL MCU Eclipse Update Site - http://freescale.com/lgfiles/updates/Eclipse/MCU10_6_4/com.freescale.mcu.updatesite

There is no problem to install MQX 4.2 plugin on line from my side.


Have a great day,
Jennie Zhang

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛

932件の閲覧回数
emanueletrapani
Contributor III

I used this site yet.

0 件の賞賛

932件の閲覧回数
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi

I tested above update link on my side. it works normally.

I wonder the problem is on your network connection.

Please change another network, or you can also try disable firewall.


Have a great day,
Jennie Zhang

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛

932件の閲覧回数
Alice_Yang
NXP TechSupport
NXP TechSupport

Hi,

Have you get the MQX installed ?

https://community.nxp.com/docs/DOC-102287  

Alice

0 件の賞賛

932件の閲覧回数
emanueletrapani
Contributor III

yes, 4.2 version of MQX.

0 件の賞賛