MKM33z128A5 for Codewarrio 10.6 bareboard project

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MKM33z128A5 for Codewarrio 10.6 bareboard project

Jump to solution
819 Views
andresbaena
Contributor II

hello

 

i need create one project for MCU MKM33Z128ACLH5, but it does not support CodeWarrior.

 

thanks

Labels (1)
0 Kudos
Reply
1 Solution
612 Views
TICS_Fiona
NXP Employee
NXP Employee

Hello andres

CodeWarrior 10.6.4 supports MKM33Z128, please see the screenshot in below for new project creating.

KM33Z.png

Please first install CW10.6.4 which can be downloaded from:

www.freescale.com/cwmcu10

Its update v10.6.5 is also available at the same link.

Further information and the release notes are available on the following Freescale community page:

https://community.freescale.com/docs/DOC-143655

Fiona Kuang

Technical Information & Commercial Support

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
1 Reply
613 Views
TICS_Fiona
NXP Employee
NXP Employee

Hello andres

CodeWarrior 10.6.4 supports MKM33Z128, please see the screenshot in below for new project creating.

KM33Z.png

Please first install CW10.6.4 which can be downloaded from:

www.freescale.com/cwmcu10

Its update v10.6.5 is also available at the same link.

Further information and the release notes are available on the following Freescale community page:

https://community.freescale.com/docs/DOC-143655

Fiona Kuang

Technical Information & Commercial Support

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply