Regarding SCI and LIN intialization in sensor MM9Z1J638

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Regarding SCI and LIN intialization in sensor MM9Z1J638

507 Views
maharajsankaran
Contributor I


Hi,

We are using the freescale S12Z family,MM9Z1J638 controller.

we are tried to intialize the SCI and LIN modules.But Regsiters are not getting intilized.

Even we tried with freescale example code.

Is there any protection for that? Please provide the detailed procedure  to initalize the SCI and LIN module.

 

Thanks in advance.

Regards,

Maharaj S

Labels (1)
0 Kudos
1 Reply

331 Views
RadekS
NXP Employee
NXP Employee

Hi maharaj,

This question was already answered by service request. For the completeness, there is last answer:

We would like to recommend using latest version of example code:

http://www.freescale.com/webapp/sps/download/license.jsp?colCode=KT9Z1-638-REFAPP

Additionally there is also official LIN2.0/2.1 driver (now called stack):

http://www.freescale.com/files/microcontrollers/software/device_drivers/FSL_LIN_2.X_STACK.zip

This stack contains also basic example codes for appropriate MCU derivatives. Please look at:

"..\FSL LIN 2.x Stack Package 4.5.4\Examples\S12Z_examples\QuIBS+Z\..


I hope it helps you.

Have a great day,
RadekS

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos