MC9S08PL16SCTG Processor Missing at Codewarrior V11.1

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MC9S08PL16SCTG Processor Missing at Codewarrior V11.1

Jump to solution
2,815 Views
egoitztoledo
Contributor III

I am traying to create a new bareboard proyect for a MC9S08PL16SCTG but I am having some troubles. I have installed the "CodeWarrior MCU 11.1 Service Pack for S08PB and S08PLS" service pack, so now, I can see the micro at the Devices list for sellection. The first problem is that at the new project assistant, the "Rapid Application Development" (image attached) step does not appear, so I can't create the project where I will be using Procesor Expert.

Furthermore, at the "Components" the processor is missing, so definetly, there is I have no way to use Processor Expert.

I wonder if these problems I am facing is a "bug" that will be solved or an intended thing. If so, I have never made a project without Processor Expert, so I would appreciate a guide or so to carri it out.

0 Kudos
Reply
1 Solution
2,806 Views
vicentegomez
NXP TechSupport
NXP TechSupport

Sorry the MC9S08PL family does not have a Processor expert  option

I really sorry

Regards

View solution in original post

0 Kudos
Reply
5 Replies
2,814 Views
egoitztoledo
Contributor III

By the way...Hello and thank you in advance.

Sorry for the oversight.

0 Kudos
Reply
2,807 Views
vicentegomez
NXP TechSupport
NXP TechSupport

Sorry the MC9S08PL family does not have a Processor expert  option

I really sorry

Regards

0 Kudos
Reply
2,798 Views
egoitztoledo
Contributor III

Hi Vicente, thank you for your answer.

It's a pitty, because as I said, I have never made a project whithout PE and I don't know how could I do it...

Dou you know if it will exist the option in a short period?

Regards.

0 Kudos
Reply
2,792 Views
vicentegomez
NXP TechSupport
NXP TechSupport

You can create a PE project for the PA family, check the configurations and copy them to a new project (without PE) for the PL

 

Sorry, but this is the only option that I have in mind

 

Regards

 

0 Kudos
Reply
2,778 Views
egoitztoledo
Contributor III

OK, thank you for your answers.

Best regards.

0 Kudos
Reply