Looking for PE Micro unit_16z.dll

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Looking for PE Micro unit_16z.dll

1,336 Views
nietsdlog
Contributor II

Hi everyone;

Someone made a patch for CodeWarrior that allowed use of USB Multilink hardware.

I lost the dll due to another WD hard drive failure (still have the patch files tho).

I've tried contacting PE but their response was "we don't keep older files like that".

Could anyone send me a copy of the DLL?   

Thanks in advance!

-E.M.

5 Replies

1,209 Views
nietsdlog
Contributor II

I know the file is from PE, my thoughts in asking were hoping one of the members might have it.

I have 3 PE interfaces, (1) Parallel, (2) USB CPU16/32 Multilink, (3) USB Multilink FX;

I'm using CodeWarrior IDE 4.1 for the Motorola HC16.

Before having to recover the hard drive I had a patch using unit_16z.dll (for the HC16) that permitted me to use the USB device(s).   This is similar to the HC12 (unit_12z.dll).   

Hoping someone might have the file :-)

0 Kudos

1,209 Views
Ben
Senior Contributor I

Hay, you took me away back in time :-) I tried to look in my old data files when I used this line, but, sorry, no success...

I hope someone still have it

Ben

0 Kudos

1,209 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

Yes, for sure it's too old. I checked my computer I don't have.

Let's leave the post here and see if someone else can help you.

1,209 Views
Ben
Senior Contributor I

Hello E.M

I am using PE USB multilink too, and have no problem with CW. Unless your CW is a very old version, or using old windows version,  try to run again the multilink_universal_install.exe file again, it should re-install the files you need for CW.

Ben

0 Kudos

1,209 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

HI, 

This file unit_16z.dll is produced by P&E, we don't have the backup.

But from your description, you meet problem of running CW with P&E tools.

What version of CW do you work with?

what's your windows platform? 

which P&E probe do you work with?

Let's see if we can help you in another way.


Have a great day,
Jun Zhang

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos