I am writing an assembly program (very basic bootloader) and wondering if there is a CPU-header file to use for assembly programs. For example, I would like to MOV the address of PORTA_PCR3 into R1. Sure, I can come up with my own header that includes everything I need but I don't want to do that if something is already provided.
Would .extern somehow work for these things?
I am using CW MCU 10.6 with a K60 CPU.
已解决! 转到解答。
Hello.
all the header file is included under
C:\Freescale\CW MCU v10.6.4\MCU\lib\wizard_data\ARM\DataBase\derivatives
MK60F15.h is also included there.
it is C type header file. not assembly. we don't have a asm syntax header file. user can use inline assembly with it.
see this url:
Extended inline assembly with GCC in CodeWarrior
can this help you?
Have a great day,
Jennie Zhang
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hello.
all the header file is included under
C:\Freescale\CW MCU v10.6.4\MCU\lib\wizard_data\ARM\DataBase\derivatives
MK60F15.h is also included there.
it is C type header file. not assembly. we don't have a asm syntax header file. user can use inline assembly with it.
see this url:
Extended inline assembly with GCC in CodeWarrior
can this help you?
Have a great day,
Jennie Zhang
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------