How to create a .srec, .hex and .elf for a S9KEAZN168 at same time in CodeWarrior?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

How to create a .srec, .hex and .elf for a S9KEAZN168 at same time in CodeWarrior?

1,377 次查看
MartinFalcon95
Contributor I

Hi, I'm trying to create an .srec, .hex and .elf for a project with an S9KEAZN168. Now I have 2 different configurations, one generate and .elf and the other one generates an .hex, but I want to generate also a .srec, and if it's possible generate the 3 in a same configuration.

0 项奖励
回复
3 回复数

1,320 次查看
MartinFalcon95
Contributor I

Thank you. Now the only problem I have is, I don't have those options, how could I add them? Thanks

MartinFalcon95_0-1679947497838.png

 

0 项奖励
回复

1,311 次查看
ZhangJennie
NXP TechSupport
NXP TechSupport

HI @MartinFalcon95 

Please check "Create Flash Image" in Additional Tool. You will see those options.

ZhangJennie_0-1679968596548.png

Have a nice day,

Jun Zhang

 

0 项奖励
回复

1,368 次查看
ZhangJennie
NXP TechSupport
NXP TechSupport

HI

You can set "Create Flash Image" to generate an image file.

ZhangJennie_0-1679552050918.png

If more type of image needed parallel,  Please combine the menthod as below

https://mcuoneclipse.com/2012/09/27/s-record-intel-hex-and-binary-files/

 

Hope this will help you.

Jun Zhang

标记 (1)
0 项奖励
回复