How to configure Codewarrior to disable eeprom erase during downloading

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

How to configure Codewarrior to disable eeprom erase during downloading

4,167 次查看
grace
Contributor I

Hello Experts,

I try to disable eeprom erase during downloading, so i configure in CW debugger window(File->Configuration->Load->click 'Advanced'->select 'EEPROM'). But the result is eeprom stil will be erased to 0 or 0xFF after downloading before the program is RUN.

ECU:PC9S12G128MLL
IDE: CW_HC12_v5.1_EVAL(download from freescale web)
Debugger firmware:P&E USB Multilink
prm setting:
SEGMENTS  /* Here all RAM/ROM areas of the device are listed. Used in PLACEMENT below. */

/* Register space  */
/*    IO_SEG        = PAGED         0x0000 TO   0x03FF; intentionally not defined */

/* RAM */
      RAM           = READ_WRITE    0x2000 TO   0x3FFF;
/* D-Flash */
      DFLASH        = READ_ONLY   0x000400 TO 0x0013FF;
·········

PLACEMENT /* here all predefined and user segments are placed into the SEGMENTS defined above. */

·········
   EEPROM_DATA   INTO  DFLASH;
END

 

Can you give the suggestion about this issue? Thanks

标签 (1)
标记 (1)
0 项奖励
回复
4 回复数

2,803 次查看
Stephen
Contributor III

In the file tree window of Code Warrior, you should have a group called "Debugger Command Files"

In there will be a "xxx_Startup.cmd" file, where "xxx" is probably the name of the programmer that you use. E.g. on my projects it is called "P&E_Multilink_CyclonePro_Startup.cmd" 

 

Insert the following lines in the file:

 

// This command skips erasing the eeprom :smileyhappy:
FLASH AEFSKIPERASING 0

 

 

Hope that helps

 

0 项奖励
回复

2,803 次查看
grace
Contributor I

Kef and Stephon,

Thanks for your help.

I modified eeprom section to NO_INIT in prm file and eeprom will not be erased. The solution is OK.

 

But i try the the second solution and it seems not work.I add 'FLASH AEFSKIPERASING 0' in P&E_Multilink_USB_Startup.cmd or P&E_Multilink_USB_Preload.cmd. EEPROM is still be erased.

Below is command window content. Is anything wrong? Thanks very much.

 

Loading Target ...
IO registers loaded for MC9S12G128 from D:\Program Files\Freescale\CWS12v5.1\prog\REG\MCU01C2.REG
USB HCS08/HCS12 MULTILINK detected - Flash Version 5.83
executing .\cmd\P&E_Multilink_USB_startup.cmd

!// At startup the commands written below will be executed
Target Ready
done .\cmd\P&E_Multilink_USB_startup.cmd

Startup command file correctly executed.
executing P&E_Multilink_USB.hwc

done P&E_Multilink_USB.hwc

executing .\cmd\P&E_Multilink_USB_preload.cmd

!// Before load the commands written below will be executed
!FLASH AEFSKIPERASING 0
done .\cmd\P&E_Multilink_USB_preload.cmd

Preload command file correctly executed.
FP: FLASH parameters loaded for MC9S12G128_V0_5(NVMIF2 rev 3,3,3,3) from D:\Program Files\Freescale\CWS12v5.1\prog\FPP\mcu01C2.fpp
USB HCS08/HCS12 MULTILINK detected - Flash Version 5.83
executing .\cmd\P&E_Multilink_USB_reset.cmd

!// After reset the commands written below will be executed
done .\cmd\P&E_Multilink_USB_reset.cmd

Reset command file correctly executed.

      MCU clock speed: 5707000 Hz
Block Module Name      Address Range   Status
   0  EEPROM             400 -  13FF   Programmed - Unselected
   1  PFLASH            1400 -  1FFF   Blank - Unselected
   2  PFLASH           88000 - FBFFF   Programmed - Unselected
   3  PFLASH            4000 -  FFFF   Programmed - Unselected

FP: The UNPROTECT command is not available for the EEPROM flash module => Skipped.

FP: The UNPROTECT command is not available for the PFLASH flash module => Skipped.

FP: The UNPROTECT command is not available for the PFLASH flash module => Skipped.

FP: The UNPROTECT command is not available for the PFLASH flash module => Skipped.
executing .\cmd\P&E_Multilink_USB_vppon.cmd

!// Before programming the flash, the commands written below will be executed
done .\cmd\P&E_Multilink_USB_vppon.cmd

Vppon command file correctly executed.

FP: The ERASE command is not performed for the EEPROM flash module (AEFSKIPERASING) => Skipped.
executing .\cmd\P&E_Multilink_USB_vppoff.cmd

!// After programming the flash, the commands written below will be executed
done .\cmd\P&E_Multilink_USB_vppoff.cmd

Vppoff command file correctly executed.
FP: Arm FLASH for loading.
executing .\cmd\P&E_Multilink_USB_vppon.cmd

!// Before programming the flash, the commands written below will be executed
done .\cmd\P&E_Multilink_USB_vppon.cmd

Vppon command file correctly executed.
executing .\cmd\P&E_Multilink_USB_vppoff.cmd

!// After programming the flash, the commands written below will be executed
done .\cmd\P&E_Multilink_USB_vppoff.cmd

Vppoff command file correctly executed.
FP: FLASH disarmed.
USB HCS08/HCS12 MULTILINK detected - Flash Version 5.83
executing .\cmd\P&E_Multilink_USB_reset.cmd

!// After reset the commands written below will be executed
done .\cmd\P&E_Multilink_USB_reset.cmd

Reset command file correctly executed.
executing E:\project\LowCostSJB\backup\bin\LowCostSJB.xpr

RESET
done E:\project\LowCostSJB\backup\bin\LowCostSJB.xpr

executing .\cmd\P&E_Multilink_USB_postload.cmd

!// After load the commands written below will be executed
done .\cmd\P&E_Multilink_USB_postload.cmd

Postload command file correctly executed.

in>

 

0 项奖励
回复

2,803 次查看
kef
Specialist I

Grace,

 

I see you added AEFSKIPERASING to preload cmd file. Try moving it to startup cmd file. If this won't work, then maybe it is not working on S12G. I used it only on S12D and it worked.

 

0 项奖励
回复

2,803 次查看
kef
Specialist I

All zeros you get because DFLASH in PRM is READ_ONLY. All variables in READ_ONLY segments are initialized. Use NO_INIT instead of READ_ONLY.

 

To make EEPROM not erased, search forums for AEFSKIPERASING. This command in debugger ini file can be used to not erase some eeprom and flash blocks.

0 项奖励
回复