How do I burn a .elf to MCF52259 from the command line? (burner.exe?)

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

How do I burn a .elf to MCF52259 from the command line? (burner.exe?)

1,055 次查看
toni_homedes
Contributor I

I'm preparing a CLI / Makefile development environment (cygwin) and I've managed to do everything up to generating an elf, but now I need to be able to

 

    burn the elf to the MCU via a script

 

and though I've found that I need to use

 

    burner.exe

 

I can't find how to properly use it. Our environment is:

 

    MCF52259 + USB ColFire(r) MultiLink / Win 7 64 bits

 

Please direct me to some manual/howto/whatever so I can learn to configure and use burner.exe

 

Thanks

标签 (1)
标记 (3)
0 项奖励
回复
4 回复数

768 次查看
BlackNight
NXP Employee
NXP Employee

You could technically use the burner.exe to flash a program to the device.

The burner.exe could output the file to a serial port.

But you would need a production programmer which has a serial port connected to that serial port.

Otherwise you need a programmer or debugger/downloader/flasher which accepts the output files(s), e.g. S19 file.

768 次查看
toni_homedes
Contributor I

Thanks Erich,

I already had the impression that the S19 was made from the elf but I didn't know way nor how. As I've said to Pascal I'll have a look at the documentation and try to find my way

0 项奖励
回复

768 次查看
trytohelp
NXP Employee
NXP Employee

Hello Toni,

The Bruner.exe tool is not a tool to flash the application on board.

This tool can be use to create the Srecord file (or bin file).

By default the entry file used is the debugger file (code + debug info).

with this file the burner will create a Srecord file.

Probably you're using the MCU v10.x tool (MCU V10.4 is the last version).

there is a doc under \CW_MCU_v10.4\MCU\Help\PDF\Build_Tools_Utilities.pdf

Please have a look page 165: Burner Utility


If you want to create a makefile or a script in order to:

- build the project,

- flash it on board.

I recommend you to refer to the Command-Line Debugger shell.

You will find some info in the CodeWarrior Common Features Guide.pdf manual.

      - page 283 -> Chapter 4 Debugger Shell,

      - page 347 -> Chapter 5 Debugger Script Migration,

      - page 30 -> 2.2 Command Line Interface

Hope this will help you.

Regards

Pascal

768 次查看
toni_homedes
Contributor I

Thanks Pascal,

I'll have a look at the documents you mention and ask back if I can't find the solution

0 项奖励
回复