FTM1 in KEA-128

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

FTM1 in KEA-128

633 Views
vigneshbalaji
Senior Contributor I

Hi,

     Is it possible to make the output of FTM 1 through an output pin ???

I tried it with FTM2 using the FTM2_OUTINIT register but i am unable to do this in  FTM1_OUTINIT since it does not have that register.

 

Is there any example of FTM1 coming out of a pin directly.

Labels (1)
0 Kudos
Reply
1 Reply

477 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello ,

I have replied you at this thread :

FTM1 - Channel 1 in KEA-128

please check !


Have a great day,
Alice Yang

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply