Down grade Codewarrior IDE from V4.7 to V4.5

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Down grade Codewarrior IDE from V4.7 to V4.5

ソリューションへジャンプ
1,369件の閲覧回数
sebikoo
Contributor I
Hello, All freescaler worldwide
 
 
I am having compile erros to complie a project made by V4.5 evaluation version 
 
at V4.7 evaluation version Thus, I have received license.dat file for V4.5 evaluation version
 
 from technical support center recently.
 
 
I currently do not have V4.5 evaluation version installation file, but only V4.7 evaluation version 
 
installation file. How could I change it to V4.5 with license.dat file received ?
 
 
Best Regards..
ラベル(1)
タグ(1)
0 件の賞賛
1 解決策
380件の閲覧回数
stanish
NXP Employee
NXP Employee
Hello sebikoo

I'd recommend you to use rather newer version since it fixes several defects.
Could you possibly specify more in detail which errors do you get?

Anyway, if you insist on v4.5 you can open Service Request and the support will send you the installer.

Stanish

元の投稿で解決策を見る

0 件の賞賛
2 返答(返信)
381件の閲覧回数
stanish
NXP Employee
NXP Employee
Hello sebikoo

I'd recommend you to use rather newer version since it fixes several defects.
Could you possibly specify more in detail which errors do you get?

Anyway, if you insist on v4.5 you can open Service Request and the support will send you the installer.

Stanish
0 件の賞賛
380件の閲覧回数
sebikoo
Contributor I
Hello Stanish
 
Errors are solved. By the way, I might face with other errors for the next weeks, because
 
this project has not been mine but others'
 
So, pls keep touch in me for later.
 
Thanks anyway for your help on this.
 
 
Regards.
0 件の賞賛