Down grade Codewarrior IDE from V4.7 to V4.5

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Down grade Codewarrior IDE from V4.7 to V4.5

跳至解决方案
1,919 次查看
sebikoo
Contributor I
Hello, All freescaler worldwide
 
 
I am having compile erros to complie a project made by V4.5 evaluation version 
 
at V4.7 evaluation version Thus, I have received license.dat file for V4.5 evaluation version
 
 from technical support center recently.
 
 
I currently do not have V4.5 evaluation version installation file, but only V4.7 evaluation version 
 
installation file. How could I change it to V4.5 with license.dat file received ?
 
 
Best Regards..
标签 (1)
标记 (1)
0 项奖励
回复
1 解答
930 次查看
stanish
NXP Employee
NXP Employee
Hello sebikoo

I'd recommend you to use rather newer version since it fixes several defects.
Could you possibly specify more in detail which errors do you get?

Anyway, if you insist on v4.5 you can open Service Request and the support will send you the installer.

Stanish

在原帖中查看解决方案

0 项奖励
回复
2 回复数
931 次查看
stanish
NXP Employee
NXP Employee
Hello sebikoo

I'd recommend you to use rather newer version since it fixes several defects.
Could you possibly specify more in detail which errors do you get?

Anyway, if you insist on v4.5 you can open Service Request and the support will send you the installer.

Stanish
0 项奖励
回复
930 次查看
sebikoo
Contributor I
Hello Stanish
 
Errors are solved. By the way, I might face with other errors for the next weeks, because
 
this project has not been mine but others'
 
So, pls keep touch in me for later.
 
Thanks anyway for your help on this.
 
 
Regards.
0 项奖励
回复