Greetings again,
In my workplace, I'm using CW6.2 in a Windows XP computer.
I have a project here that compiles fine and works fine too.
But when I try to compile it at home, where I have a CW6.3 running on a Windows Vista, it gives me an error saying it has a 32 file limitation (I'm not sure it was actually 32 files).
Is that right? If I upgrade my CW here at work, will my projects stop compiling?
I don't think that matters, but at home I also have CW7.2 installed. Here at work I installed it in a different computer because a colleage has warn me about possible conflicts. But tjat's really unconfortable...
Please let me know if these simptoms make sense to you guys.
Thanks a lot.
已解决! 转到解答。
What you are running into is a licensing problem. Your copy of CodeWarrior at work is licensed, and has no limitations. You are probably running the Special Edition of CodeWarrior at home, and it has limitations, typically either the number of files it can hande or the amount of code that can be generated.
---Tom
What you are running into is a licensing problem. Your copy of CodeWarrior at work is licensed, and has no limitations. You are probably running the Special Edition of CodeWarrior at home, and it has limitations, typically either the number of files it can hande or the amount of code that can be generated.
---Tom