Convertion from >DIR to .mov

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Convertion from >DIR to .mov

跳至解决方案
1,620 次查看
viji
Contributor I
Hi there,

Is there any way to convert .DIR and respective .AUD files to QT movie file?
I have a set of .DIR and .AUD files, which I want to play using Quicktime player.

Thanks for any help.

Viji

Message Edited by viji on 2007-06-25 05:27 AM
标签 (1)
标记 (1)
0 项奖励
回复
1 解答
643 次查看
J2MEJediMaster
Specialist I
You're talking about converting media files for QuickTime. I'm not sure this is the appropriate forum for this, as CodeWarrior tools are oriented towards embedded work now. You want to go to the Apple Developer forums at http://developer.apple.com/, or alternately, Google for media convertor utilities.

---Tom

在原帖中查看解决方案

0 项奖励
回复
2 回复数
643 次查看
CrasyCat
Specialist III
Hello
 
I am not sure you are on the appropriate Forum here.
 
- Which CPU are you targeting (HC08, HC12, Coldfire, ..)
- Which version of CodeWarrior are you using?
  To retrieve that info:
    - Start CodeWarrior
    - Select Help -> About Freescale CodeWarrior
    - Click on "Install Products"
    - CodeWarrior version used is displayed on top in the Installed Products dialog.
CrasyCat
0 项奖励
回复
644 次查看
J2MEJediMaster
Specialist I
You're talking about converting media files for QuickTime. I'm not sure this is the appropriate forum for this, as CodeWarrior tools are oriented towards embedded work now. You want to go to the Apple Developer forums at http://developer.apple.com/, or alternately, Google for media convertor utilities.

---Tom
0 项奖励
回复