CodeWarrior V11.1, Hiwave.exe was not found!

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

CodeWarrior V11.1, Hiwave.exe was not found!

1,391件の閲覧回数
lelam
Contributor II

Hi guys,

We developing S08 family. We have 2 problems during production, please help us clear it.
1. Is there a way we can flash program without a project code,  just need to send the image file .abs, hex and Mutilink Universal FX or USBDM kit production department.
Is it possible to use Hiwave.exe, right? but we using CodeWarrior V11.1, and we don't find it ..maybe it's only in < V6.3

2. We want to lock the image file from our product (copy protection program), can we do it?

Thank you!

ラベル(1)
5 返答(返信)

1,165件の閲覧回数
ErichStyger
Senior Contributor V

Hi,

1) how to flash in standalone mode: Standalone Flash Programmer | MCU on Eclipse 

Or you can use the IDE in scripting mode, see Programming Kinetis with CodeWarrior from the DOS Shell | MCU on Eclipse 

2) Yes, check your device manual about flash protection and read out protection. See for some information about this: Preventing Reverse Engineering: Enabling Flash Security | MCU on Eclipse 

I hope this helps,

Erich

1,165件の閲覧回数
lelam
Contributor II

Hi,

Thank you, it helped me a lot.
1. Flash File to the Target is a good choice for me now
2. Yes, in CW, I have Enable Security Flash
In another your topic about it: https://mcuoneclipse.com/2012/11/04/how-not-to-secure-my-microcontroller/
Are there any note I should pay attention to when using it? I use MC9S08PT
Thank you very much!

Flash Security.PNG

22.PNG

0 件の賞賛

1,165件の閲覧回数
ErichStyger
Senior Contributor V

other than that, search for applicable application notes (your search engine is your friend here). For example the attached one.

Erich

0 件の賞賛

1,165件の閲覧回数
soledad
NXP Employee
NXP Employee

Hi, 

hiwave.exe is only for CW classic. 

I suggest to check the following link: 

https://community.nxp.com/thread/60277 

I hope this helps, have a nice day!

1,165件の閲覧回数
lelam
Contributor II

Hi,

Yes, I am referencing it. Thank you so much!

0 件の賞賛