CW4.5 - S12XDP512 - Debug Error

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

CW4.5 - S12XDP512 - Debug Error

跳至解决方案
2,771 次查看
Arindam
Contributor I
Hello,
 
While debugging a part of code I am getting this message in command window.
 
FCS Warning (ID 25): writing to reserved register at pc = 0xfe8041'L. Value: 0xFE, Memory Address: 0x5. MEBI module is affected
 
Can someone tell me why does this come what could be the possible solution.
 
TIA.
Arindam

--
Alban Edit: Please always include FSL Part Number in Message Subject line.



Message Edited by Alban on 2007-09-17 10:31 AM
标签 (1)
标记 (1)
0 项奖励
回复
1 解答
1,010 次查看
CrasyCat
Specialist III
Hello
 
If you have submitted a Service Request for that, you should get an answer from one of our support engineer.
 
CrasyCat

在原帖中查看解决方案

0 项奖励
回复
7 回复数
1,010 次查看
Alban
Senior Contributor II
Hello Arindam,

I'm afraid I don't have much information to help you.
However, the message seems clear to me:

Your application is writting where it should not because it is reserved space.

It's all I can say with what you gave.

Cheers,
Alban.
0 项奖励
回复
1,010 次查看
Arindam
Contributor I
Hello,
 
Just to add to the previous details, I am not testing the code on target but only on simulator. So anyone having a CW can also reproduce the bug, with the project provided by me on request, and try and analyse. Just for information I have raised a service request as well with Request Number 1-387190247.
Anyone having access to that also can go through it as i have sent my project also on that request no.
 
Cheers,
Arindam.
0 项奖励
回复
1,011 次查看
CrasyCat
Specialist III
Hello
 
If you have submitted a Service Request for that, you should get an answer from one of our support engineer.
 
CrasyCat
0 项奖励
回复
1,010 次查看
Arindam
Contributor I
I am working on CW 5.7.1 and build the project for MC9S12XDP512 platform and I am using CW debugger.


Message Edited by Arindam on 2007-09-14 11:50 AM
0 项奖励
回复
1,010 次查看
CrasyCat
Specialist III
Hello
 
Which version of CodeWarrior are you using?
To retrieve that info:
   - Start CodeWarrior
   - Select Help -> About Freescale CodeWarrior
   - Click on "Install Products"
   - CodeWarrior version used is displayed on top in the Installed Products dialog.
 
I assume you are debugging in the simulator.
Which device simulation module did you load?
To retrieve that info:
   - Start the simulator the usual way
  - Select "HCS12X FCS" -> "Set Derivative"
    What is written there? 
 
CrasyCat
0 项奖励
回复
1,010 次查看
Arindam
Contributor I
Well as mentioned earlier I am using MC9S12XDP512 derivative and the CW version is HC12 4.5, Build 6037.
0 项奖励
回复
1,010 次查看
Lundin
Senior Contributor IV
You might want to post relevant info such as which cpu, which debug/programming tool and which CW version you are using.
0 项奖励
回复