CW 10.7 56800/E, HOW DO I add second s-record and\or symbol table to debug session?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

CW 10.7 56800/E, HOW DO I add second s-record and\or symbol table to debug session?

534 次查看
elvismemphis
Contributor I

The DSC 56F800 debugging seems very primitive.

 

In CW 10.7 I do not see how to add a second s-record to flash in the debug session. Further, I do not see a method to load a second symbol table. These features are very useful when debugging bootloader & application scenarios.

 

Also, I do not find any discrete control for how much flash to erase (sector control). The flash programmer that comes with CW 8.3 does provide unit, all, or page. That is helpful but still pretty course.

 

What are the steps to add a second s-record or a symbol table to an existing debug session?

Is there any discrete control over the flash programming process (like TI Code Composer 3.3 which is also old vintage)?

0 项奖励
1 回复

416 次查看
BlackNight
NXP Employee
NXP Employee

Hi Elvis,

see Adding Symbols to the CodeWarrior Debugger | MCU on Eclipse  how you can add symbols to a debug session with CodeWarrior.

I hope this helps,

Erich

0 项奖励