CFFLASHER alternative in Windows 7 / 10 to burn .S19

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

CFFLASHER alternative in Windows 7 / 10 to burn .S19

ソリューションへジャンプ
3,025件の閲覧回数
ssinfod
Contributor IV

Hello,

 

I own some BDM tools from P&E Micro.

Model: "USB-ML-CFE" BDM.  (http://www.pemicro.com/products/product_view.cfm?product_ID=163)

I also have the Cyclone PRO and also some boards with integrated BDM. (ex: M52233DEMO)

 

We are mainly using the CFFLASHER tool on Windows XP or Windows 7 (32 bits) to burn our (coldfire) .S19 file.

 

Here are my questions:

 

Is there any plan from Freescale/NXP to update CFFLASHER for Windows 7 (64 bits) or Windows 10 ?

If not, would it be possible to release the source code of CFFLASHER on this forum (or github / sourceforge)  ?

Otherwise, can you suggest alternative software for CFFLASHER for Windows 7 or 10 ?

 

Can I use CodeWarrior 10.x to burn a .S19 file to any Coldfire processor ?

Is there a "burn/program" tool within CodeWarrior 10.x ?

 

Thanks for your answer,

ssinfod

ラベル(1)
0 件の賞賛
返信
1 解決策
2,140件の閲覧回数
TICS_Fiona
NXP Employee
NXP Employee

Hello ssinfod

Unfortunately the CFFlasher does not support Windows 7. It only works on Windows XP or 2000.

You can use the Flash Programmer in CodeWarrior v10.6.4.  CW10.6 can be downloaded from:

http://tinyurl.com/6jo5tge

To program Coldfire in CW10.6 IDE, you may create a Target Task for flash programmer, or use the 'Flash File to Target' feature.

For details, please view the section <Debugger->Flash Programmer> in v10.x FAQ Guide:

C:\Freescale\CW MCU v10.6\MCU\Help\PDF\Microcontrollers_FAQ_Guide.pdf

To use it as a standalone tool, please see below for how to do it:

http://mcuoneclipse.com/2012/08/02/standalone-flash-programmer/

Here is CodeWarrior Flash Programming from a DOS Shell

http://mcuoneclipse.com/2012/08/03/codewarrior-flash-programming-from-a-dos-shell/

Best Regards

Fiona Kuang

Technical Information & Commercial Support

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Mark Correct button. Thank you!

  ---------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
2,141件の閲覧回数
TICS_Fiona
NXP Employee
NXP Employee

Hello ssinfod

Unfortunately the CFFlasher does not support Windows 7. It only works on Windows XP or 2000.

You can use the Flash Programmer in CodeWarrior v10.6.4.  CW10.6 can be downloaded from:

http://tinyurl.com/6jo5tge

To program Coldfire in CW10.6 IDE, you may create a Target Task for flash programmer, or use the 'Flash File to Target' feature.

For details, please view the section <Debugger->Flash Programmer> in v10.x FAQ Guide:

C:\Freescale\CW MCU v10.6\MCU\Help\PDF\Microcontrollers_FAQ_Guide.pdf

To use it as a standalone tool, please see below for how to do it:

http://mcuoneclipse.com/2012/08/02/standalone-flash-programmer/

Here is CodeWarrior Flash Programming from a DOS Shell

http://mcuoneclipse.com/2012/08/03/codewarrior-flash-programming-from-a-dos-shell/

Best Regards

Fiona Kuang

Technical Information & Commercial Support

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Mark Correct button. Thank you!

  ---------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信