Hello chunhua
User can download the example projects for 56F84789 from:
MC56F84xxx|Digital Signal Controllers|NXP
The example package is under ‘Software Development Tools -> Lab and Test Software’ in the above page.
It contains the example projects for CAN and SCI driver which are both based on PE.
The flash security operations are same on 56F84xxx and Kinetis products, so you can refer to this document:
http://cache.nxp.com/files/microcontrollers/doc/app_note/AN4507.pdf
User can still reprogram the 56F84xxx after flash is secured, just mass erase the flash before reprogramming.
Hope this helps!
Best Regards
Fiona Kuang
TIC - Technical Information Center
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Mark Correct button. Thank you!
-----------------------------------------------------------------------------------------------------------------------