您好!
我下载了MC56F84789的程序,但是我无法看懂,请你们给一份使用C语言编写的,2个控制板子之间,实际能够通信的实用程序,基于can网和串行口通信程序,最好使用专家系统的例子程序。
如何设置MC56F84789的保密,同时又可以重新烧写。
祝好!
您好!
请问,你说的,要我下载的软件代码文件编码是不是MC56F84XXXSW 呢?这个软件我早就下载下来了,我看不懂这个里面的代码,请你们给我提供一份比较实用的CAN网和通用串行通信代码,不是用于测试MC56F84789内部寄存器的代码,主要是代码里面需要有各寄存器的配置代码。
加密文档,我已经下载下来了,若有问题,再咨询你们。
祝好!
Hello chunhua
User can download the example projects for 56F84789 from:
MC56F84xxx|Digital Signal Controllers|NXP
The example package is under ‘Software Development Tools -> Lab and Test Software’ in the above page.
It contains the example projects for CAN and SCI driver which are both based on PE.
The flash security operations are same on 56F84xxx and Kinetis products, so you can refer to this document:
http://cache.nxp.com/files/microcontrollers/doc/app_note/AN4507.pdf
User can still reprogram the 56F84xxx after flash is secured, just mass erase the flash before reprogramming.
Hope this helps!
Best Regards
Fiona Kuang
TIC - Technical Information Center
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Mark Correct button. Thank you!
-----------------------------------------------------------------------------------------------------------------------