when in debug mode, the arrow only in assemble code window

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

when in debug mode, the arrow only in assemble code window

1,466 Views
hansonlv
Contributor I

I use codewarrior5.1 . I copy a program from linda, and the program work well on her computer,but when i went into debug mode,some message appeared as"C:\Users\linda\Documents\ Projects\source\main.c could not found". I have been make the program, but why the information about linda appeared?

 

when i open the main.c ,there is no arrow in main.c, but i can see there is a arrow in assemble window. How can i do, anyone can give some advice, thank you all.

Labels (1)
0 Kudos
Reply
1 Reply

1,413 Views
trytohelp
NXP Employee
NXP Employee

Hi,

Do you have access to the main.c source file ?.

By default the .abs file contains the debug information and the paths of all source files using in an application.

However if the path changed or if the file is not found, only assembly code will appear.

How to solve it ?

Better is to have the full application or your PC and to re-build the project.

Then the path will be defined according to your PC project location.


Have a great day,
Pascal
Freescale Technical Support
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply