I'm using the "Flash File To Target" utility of CW 10.5 for K60 and get failure "0 Bytes Programmed, Check Restricted Address Range". Code works fine in debug/RAM and debug/FLASH but I cannot write my application to flash. Where should I look to fix this? I tried to modify the target task by un-checking the "Restrict to Addresses in this Range" box but this didn't help.
Thanks!
解決済! 解決策の投稿を見る。
Hi Thomas:
If program only works in debug mode, it could be caused by library selection:
Regards!,
Jorge Gonzalez
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hello Jorge Gonzalez,
I got the same problem. But when I tried to do the changes as request, it didnt work. Fyi, I am using the MK30DX256VLL7. Is there any other possibility that may cause this?
Thank you very much.
Hello norzilah abu bakar:
What do you mean with "the same problem"?
Please create a new post in the space CodeWarrior Development Tools and provide details about your issue.
Regards!
Jorge Gonzalez
Hello Thomas:
Do you get a "Program Command Succeeded" kind of message in the console? It sounds like the next cases:
Re: K60 flash programming problem
Please help: flash to target results in 0 bytes programmed
First thing to check is that the file you want to flash actually has some information to be loaded to "Flash" space (e.g. that you are not selecting a file from the [RAM] build folder)
Regards!,
Jorge Gonzalez
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hello Jorge:
Thank you for your response. I ended up deleting the build configurations and re-creating them from scratch. That seemed to get the flash utility to download the image to flash. Unfortunately the program will not run from reset so I have that piece to work out at the moment. Running in debug mode works fine.
Hi Thomas:
If program only works in debug mode, it could be caused by library selection:
Regards!,
Jorge Gonzalez
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Thank you very much, Jorge! That resolved the final issue.
Best regards,
Tom