Project upgrade from CodeWarrior 6.3 to 7.2

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Project upgrade from CodeWarrior 6.3 to 7.2

592 Views
kameliabakiri
Contributor I

Dear NXP support team,

 

Currently I'm working on the upgrade of a software project that was created with CodeWarrior 6.3 to CodeWarrior 7.2.

I would like to know about the changes that were made from 6.3 to 7.2 in order to evaluate the feasibility of the upgrade.

Is there any risk that could be introduced by this operation ?

 

 

I thank you in Advance.

 

Regards,

Kamelia BAKIRI

Firmware Engineer

Schlumberger – SRPC

1 rue Henri Becquerel, BP 202 – 92140 Clamart Cedex France

Phone: 01 45 37 24 41

Labels (1)
0 Kudos
Reply
1 Reply

472 Views
TICS_Fiona
NXP Employee
NXP Employee

Hello Kamelia

There are 2 TNs under the V7.2 installation.

Please refer to the \CodeWarrior for ColdFire V7.2\Help\PDF folder.
The TN256.pdf and TN268.pdf give some info to move from V6.x to V7.2.

I also attached them.

Best Regards

Fiona Kuang

TIC - Technical Information Center

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Mark Correct button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply