CW installs in W10/32.
The dongle licensing procedure fails.
License files that work in Windows XP seem to be in error.
CW will not install in W10/64.
Setup fails, and says nothing was installed.
No reason is given.
Why is Windows 10 such a problem?
What is needed to resolve this?
For 8bit MCU, we recommend CW11
CodeWarrior® for Microcontrollers-Eclipse IDE 11.1 | NXP
For 16bit MCU, we recommend CW5.2
CodeWarrior® Dev Tools for HCS12(X) MCUs | NXP
above two versions can support win10.
Hi,
Not so good news concerning CW6.3
Good news however, concerning CW5.2.
Q1: Where can I download CW5.2?
Q2: Will my 4.7 license.dat work with CW5.2?
Q3: If not, please send a license.dat for CW5.2, with the same 4.7 capabilities.
Please find current license.dat for 4.7 attached.
/Anders J
Från: ZhangJennie
Skickat: den 19 augusti 2019 07:58
Till: Anders Johansson
Ämne: Re: - Re: How is CW V6.3 & V4.7 installed in Windows 10, 32/64 bit?
<https://community.freescale.com/resources/statics/1000/35400-NXP-Community-Email-banner-600x75.jpg> NXP Community
Re: How is CW V6.3 & V4.7 installed in Windows 10, 32/64 bit?
reply from ZhangJennie <https://community.nxp.com/people/ZhangJennie?et=watches.email.thread> in CodeWarrior Development Tools - View the full discussion <https://community.nxp.com/message/1192923?commentID=1192923&et=watches.email.thread#comment-1192923>
CW6.3 and 4.7 doesn't support win10.
do you start a new project or work on the old project? these two versions are too old. are those the must for you?
I would recommend new versions that can support win10 for you based on your chip.
Have a great day,
Jun Zhang
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------