How is CW V6.3 & V4.7 installed in Windows 10, 32/64 bit?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How is CW V6.3 & V4.7 installed in Windows 10, 32/64 bit?

2,463 Views
AndersJ
Contributor IV

CW installs in W10/32.

The dongle licensing procedure fails.

License files that work in Windows XP seem to be in error.

CW will not install in W10/64.

Setup fails, and says nothing was installed.

No reason is given.

Why is Windows 10 such a problem?

What is needed to resolve this?

Tags (2)
0 Kudos
Reply
5 Replies

2,216 Views
AndersJ
Contributor IV

I need to support old projects, and possibly create new ones.

Which Codewarrior versions for the above chips run under Windows 10?

0 Kudos
Reply

2,216 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

For 8bit MCU, we recommend CW11

CodeWarrior® for Microcontrollers-Eclipse IDE 11.1 | NXP 

For 16bit MCU, we recommend CW5.2

CodeWarrior® Dev Tools for HCS12(X) MCUs | NXP 

above two versions can support win10.

0 Kudos
Reply

2,216 Views
AndersJ
Contributor IV

Hi,

Not so good news concerning CW6.3

Good news however, concerning CW5.2.

Q1: Where can I download CW5.2?

Q2: Will my 4.7 license.dat work with CW5.2?

Q3: If not, please send a license.dat for CW5.2, with the same 4.7 capabilities.

Please find current license.dat for 4.7 attached.

/Anders J

www.firefly.se

Från: ZhangJennie

Skickat: den 19 augusti 2019 07:58

Till: Anders Johansson

Ämne: Re: - Re: How is CW V6.3 & V4.7 installed in Windows 10, 32/64 bit?

<https://community.freescale.com/resources/statics/1000/35400-NXP-Community-Email-banner-600x75.jpg> NXP Community

Re: How is CW V6.3 & V4.7 installed in Windows 10, 32/64 bit?

reply from ZhangJennie <https://community.nxp.com/people/ZhangJennie?et=watches.email.thread> in CodeWarrior Development Tools - View the full discussion <https://community.nxp.com/message/1192923?commentID=1192923&et=watches.email.thread#comment-1192923>

0 Kudos
Reply

2,216 Views
BlackNight
NXP Employee
NXP Employee

The downloads are  here:

CodeWarrior Downloads | NXP 

I hope this helps,

Erich

0 Kudos
Reply

2,216 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi Anders Johansson

CW6.3 and 4.7 doesn't support win10.

do you start a new project or work on the old project? these two versions are too old. are those the must for you?

I would recommend new versions that can support win10 for you based on your chip.


Have a great day,
Jun Zhang

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply