How do I download Metrowerks CodeWarrior for ColdFire v4.0.2.4 (IDE V5.2.1174)?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

How do I download Metrowerks CodeWarrior for ColdFire v4.0.2.4 (IDE V5.2.1174)?

996 次查看
regelseuguh
Contributor I

How do I download Metrowerks CodeWarrior for ColdFire v4.0.2.4 (IDE V5.2.1174)?

标签 (1)
标记 (1)
0 项奖励
3 回复数

713 次查看
TICS_Fiona
NXP Employee
NXP Employee

Hello Hugues

ColdFire v4.0.2.4 is a very old version, first you need to install v4.0, then install its update v4.0.1 and v4.0.2.

Do you need all of them or only v4.0.2 update? 

Best Regards

Fiona Kuang

Technical Information & Commercial Support

0 项奖励

713 次查看
regelseuguh
Contributor I

Yes, I need all of them.

“Only through the bringing together of head and heart—intelligence and goodness—shall man rise to a fulfillment of his true nature.”

0 项奖励

713 次查看
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi Hugues,

Coldfire v4.0 is too old, I don't think it's still available on external website.

please summit a case to NXP support system. we can send it to you via transweb.

regarding to how to summit case:

How to log an issue in Case system instead CRM (Service request - not used anymore)?

here is to download update v4.0.1 and v4.0.2

CodeWarrior Updates for Coldfire v6.2 & older|NXP


Have a great day,
Jennie Zhang

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励