Exclamation marks in Device manager, Failure message in CodeWarrior

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Exclamation marks in Device manager, Failure message in CodeWarrior

746 Views
laszlo_torok
Contributor I

Hi !
I connected an S9S12GA128 uC to the Multilink Universal FX debugger and installed a CodeWarrior CWS12v5.2 on my W10 Op.Sys in order to flash it. The PC has not recognized the debugger appropriate because in the device manager can any exclamation marks be seen. I did any times driver update but the situation is the same:

pastedImage_3.png

In CodeWarrior after loading Projekt File and doing 'Debug' there is next message coming:

pastedImage_4.png

What would you recommend to do ?

Thanks.

Laszlo

Labels (1)
3 Replies

649 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello Laszlo,

Please try to install latest PEmicro drivers

http://www.pemicro.com/downloads/download_file.cfm?download_id=53

and firmware for S12(X) :

http://www.pemicro.com/downloads/download_file.cfm?download_id=346 

There is a similar question you can have a look:

How to use P&E USB Multilink with 9S12XE and CW 5.2? 

Have a great day,
TIC

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

649 Views
laszlo_torok
Contributor I

Hello Alice,

thanks for the suggestions, in the end the firmware update has helped.

The new device 'pemicrowindrvr' in Jungo appeared and the exclamation marks disappeared except WinDriver in the Device Manager, see below:

pastedImage_1.png

It was possible to flash the uC.

Thanks once more, regards:

Laszlo

0 Kudos

649 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello Laszlo,

Ok, good to hear it can work.


Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos