Error launching p2020-core00_RAM-P2020_Connect 라는 에러가 납니다.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Error launching p2020-core00_RAM-P2020_Connect 라는 에러가 납니다.

1,183 Views
kimyoungho
Contributor I

'Launching p2020-core00_RAM_P2020_Connect' has encountered problem.

Error launching p2020-core00_RAM_P2020_Connect CCSProtocolPlugin : Could not connect to the probe

(or other debug link) [CCS last  error : CC driver failure]

 

이런 메시지가 나오면서 연결이 안되는데 케이블 연결등은 모두 정상인데 어떤 이유에서 이런 에러가 발생하는지

도움 부탁드립니다.

Labels (1)
0 Kudos
Reply
4 Replies

937 Views
yipingwang
NXP TechSupport
NXP TechSupport

Hello Kim YoungHo,

There is problem with CCS USB driver. Do you use CodeWarrior TAP or USB TAP?

CodeWarrior TAP integrates both USB and Ethernet ports. USB TAP is the old product, only integrates USB port.

In addition, do you use CodeWarrior 10.5 and Windows 7 OS?


Have a great day,
Yiping

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

937 Views
kimyoungho
Contributor I

Dear,

We have used CodeWarrior 10.5 and Windows 7 OS.

Please See attached file carefully and send to us best solution.

Best regards.

0 Kudos
Reply

937 Views
yipingwang
NXP TechSupport
NXP TechSupport

Hello KEYIDEA YoungHo,

Please refer to the following hardware design.

Ensure HRESET not tied to TRST, and HRESET to the processor exclusive to COP/JTAG header.


Have a great day,
Yiping

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

937 Views
kimyoungho
Contributor I

Dear

P2020 ASLEEP pin always high.

How can I solve this problem?

Thanks & Best regards

0 Kudos
Reply