Hi,
I am working on mpc5125 board and code warrior v9.2. when i run the example program say hello world program, the program compiles, gets downloaded to the board and executes. But i dont see any output window being created on my monitor screen to view the result of printf statement. where do i view these results ??
解決済! 解決策の投稿を見る。
Hi Lander,
i had actually forgotten to read the tutorial document that comes along with the board. To view the printf statement results,
Bitsper Second: 115200, Data bits: 8, Parity:None, Stop bit: 1, Flow control: None.
After you run the program printf statement results can be seen in the hyper terminal !!
I'm having the same issue with the twr-k60d100m. I've been searching online for others with similar issues and it is hard to find the solution. Apparently in 2011, CodeWarrior console did not support printing to the console in MQX, not sure if it still holds today.
Hi Lander,
i had actually forgotten to read the tutorial document that comes along with the board. To view the printf statement results,
Bitsper Second: 115200, Data bits: 8, Parity:None, Stop bit: 1, Flow control: None.
After you run the program printf statement results can be seen in the hyper terminal !!
I am able to debug the program but the trouble I am facing still is the printf()'s in the terminal. When I go to my Device Manager, the only device that shows up is named, LibUSN-Win32 Devices and inside is Open Source BDM - Debug Port, and there are no options to change the bits per second, data bits...etc inside that device properties. What am I doing wrong?
Thank you,
Lander
Hi,
Once you connect your board's usb port to your pc, the com port should get detected under device manager - ports(COM and LPT). If not there should be some driver issues which can be sorted out by installing the device driver
Freescale_CDC.inf. (this driver file can be downloaded from the net).
And the settings for bits per second, data bits...etc should be made in the microsoft's hyperterminal program. You cannot do it in the device manager.
The printf() results will be seen in the hyper terminal window after you run your program.
I tried looking for the Freescale_CDC.inf on the net and I was not successful. In my research for looking for the Freescale_CDC.inf, I came across some discussions on the USB CDC is not compatible yet with Windows 8. I am running a Windows 8 - 64 bit machine, do you have any advice? If Windows 8 is not compatible, do you know when they might me?
You have been of great help, thank you a lot!
Lander
The procedure what i have mentioned in the previous discussions has worked fine for my board ( TWRMPC5125).
Am not very sure about windows 8 - 64 bit machine.
If you need further clarifications you can always raise a technical request.
hi
champaka
I am working on mpc8313 board and code warrior v8.8. when I run the example program say hello world program, the program compiles, gets downloaded to the board and executes. But I saw something incorrect output on my hyper-terminal. what’s wrong??
I have made the Serial port setting both on the terminal and the Freescale CW the same :
the output on the terminal:
the programe is just a helloworld:
printf("Hello World !\r\n"); |
can you what's wrong ?
thank you
bin
Hello
Did you check the file 8313_RDB_Readme.txt located in the Documentation folder?
The settings required for the serial port on your Host PC are described in this file..
CrasyCat
hello
i have just done as the 8313_RDB_Readme.txt:
Data rate :115200bps
Number of Data bits :8
Parity : None
Number of Stop bits :1
Flow Control : Hardware / None
bin
Hello
That is strange.
I created a project for 8313 RDB board and the connection settings are as follows:
Baud Rate: 57600
Data Bits: 8
Parity: None
Stop Bits: 1
Flow Control: None
I am running CodeWarrior for Power Architecture V8.8.5.
Can you try with this configuration?
CrasyCat
Pefect ! it is so strange ! thank you , CrasyCat ! The output is right !
bin
When u get this, just press the reset button on your board and do it all over again.. ( close ur hyper terminal window n open a new connection, debug ur program using J- Tag once again )
Rookie mistake. I got it now!
hi
i have just tried it again and again , but i still just get some messy code .
bin