MC56F8035 support on CodeWarrior for DSC 8.3

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MC56F8035 support on CodeWarrior for DSC 8.3

896件の閲覧回数
PhilC69
Contributor II

Hi,

 

i'm using two 56F8025 on my prototype board and one is memory full, so i upgraded with a 56F8035 (64k flash instead of 32k).

When i want to add a new cpu in my project, the 56F8035 is not available.

I'm using CodeWarrior for DSC 8.3 with Processor Expert 3.00 patch 02 and i have a standard license.

How can I add this cpu to prrocessor Expert ?

 

Thanks

ラベル(1)
0 件の賞賛
返信
1 返信

730件の閲覧回数
vfilip
NXP Employee
NXP Employee

Hello,

unfortunately 56F8027/33/35 MCUs are supported only in CW V10.2 and newer.

http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=CW-MCU10&tid=CWH

best regards

Vojtech Filip

Processor Expert Support Team


0 件の賞賛
返信