initialise port for writing the code

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

initialise port for writing the code

1,016 Views
koka
Contributor I
hi ...
i 'm new to this DSP56F801 digital signal controller....
i don't know about DSP coding...
but i'm familiar with c language and i want to prefer c and asm for writing the DSP code...
so want to start code....so please help him....how to start the code like initialisation of port and usage of GPIO etc ....
if possible anyone can provide code ( C & asm) for any small application....i will be so much thank full...
and if possible provide tips for writing the code....




Labels (1)
Tags (1)
0 Kudos
Reply
1 Reply

263 Views
trytohelp
NXP Employee
NXP Employee

Hi,

 

Delivered on the installation there are lot of examples.

Please refer to the folder: \(CodeWarrior_Examples)

 

Other examples are available under the project Wizard: File ¦ New under the IDE.

Project can be found in the folder: \Stationery

 

The tool includes Processor Expert (code generator).

This could be usefull.

There are some examples using it and you can change the processor used.

Generic example is in : \Stationery\Processor_Expert

 

Hope this will help you. 

 

Regards

Pascal

0 Kudos
Reply