Hello,
I am curious that what are the banked memory and non-banked memory?
As a result of my research, the banked memory is logical unit that can be accessed independently by a dividing the storage device.
However, i didn't find any non-banked memory. I just found it to be a defined interrupt memory area.
So I am more curious about the non-banked memory and banked memory.
解決済! 解決策の投稿を見る。
Hi
NON banked memory can be accessed by 16bits address. For example below is nonbanked address:
RAM 0x2000 TO 0x3FFF;
EEPROM 0x0C00 TO 0x0FFF;
ROM_4000 0x4000 TO 0x7FFF;
ROM_C000 0xC000 TO 0xFEFF;
Some parts of an application must always be in non–banked memory, in particular:
Have a great day,
Jun Zhang
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------
Hi
NON banked memory can be accessed by 16bits address. For example below is nonbanked address:
RAM 0x2000 TO 0x3FFF;
EEPROM 0x0C00 TO 0x0FFF;
ROM_4000 0x4000 TO 0x7FFF;
ROM_C000 0xC000 TO 0xFEFF;
Some parts of an application must always be in non–banked memory, in particular:
Have a great day,
Jun Zhang
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------
Thanks you for reply my question.
I understood the example by explaining it. Thanks.
Have a happy day,
Ji Hyun.
You are welcome!
8 and 16-bit CPUs like S08 or other than S12Z S12's have 16-bits address pointer registers. This limits normal address space to 2^16 = 64k. What easily fits this 64k space could be nonbanked or nonpaged. To access more than 64k memory is organized into banks or pages. Some fraction of 64k space is page window, you switch page number to map different piece of memory to selected page window. This is banked or paged memory. And coming back to nonbanked/nonpaged def., more strictly it is part of memory which has no memory page windows and thus can be uniquely addressed by 16-bit (CPU) address.
Thanks comment my question.
I don't know if I understood well. So I have questions.
Is it non-banked or non-paged to access memory space(64k)? And when accessing more than the space of memory, is it a banked or a paged memory?
Have a nice day,
Ji Hyun
Yes
Thanks you,
I understood about non-banked and banked.
Have a great day :smileyhappy:
Ji Hyun