You need to define one of the options either in a header file or better yet right on the command line. You can do this in the project / target settings. Open your project in the IDE then select the Edit menu. From there, find your project settings. This should be near the bottom of the list. The target settings dialog should now open. In the Target settings panel under the Target item select Compiler for HC08. Press the Options button. The Compiler Option Settings dialog will open. Select the Language tab. Select and check the Processor Definitions item and type one of the definitions in the control box. Your options are:
HID_MOUSE
HID_KBD_DEMO
HID_JOYSTICK_DEMO
USB_CDC
HID_DEMO
Close the dialog and re-compile.
John Pavlick