Error:  Couldn't download flash driver file while trying to erase flash memory

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Error:  Couldn't download flash driver file while trying to erase flash memory

1,150 次查看
EricoVieiraPort
Contributor I

Hello,

 

I'm trying to erase flash using flash programmer task action, but I'm getting the following error:

 

Error: Couldn't download flash driver file.Not enough memory allocated for the flash driver. Please allocate at least 0x00004370 b
ytes of Target Memory Buffer Space on the Target Configuration page.

 

I've seen the Target Configuration Page on some very outdated documents on internet, but it seems it doesn't exist in my code warrior version - I have the latest. I'm using USP TAP in a board using MPC8323E and my flash memory is a JS28F256. I can read the memory fine - did a flash dump to save the actual content.

 

Other than that, is there any simpler software to use with USB TAP? Code Warrior is a heavy load on my computer and I don't need it since I'm building my envinronment using LTIB. I'm on Ubuntu 11.10. I just need USB TAP to erase/program my bootloader (using u-boot generated with ltib).

 

Regards

标签 (1)
0 项奖励
回复
1 回复

521 次查看
EricoVieiraPort
Contributor I

Downloading Flash Diagnostics Driver ...
Reading flash ID ...
Running Diagnostics ...
Error: The Diagnostics operation failed. Flash diagnostics reports the following error(s): Operation Unsupported
Error: Diagnose operation failed

 

I can't do nothing, wth?

0 项奖励
回复