Custom Linker Section, recognized in assembly

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Custom Linker Section, recognized in assembly

跳至解决方案
1,225 次查看
Kerrie
Contributor I

We have a project using a mix of C and Assembly on the Coldfire V1, QE256 part.

 

Using the App Note AN4329, I was able to create a custome linker section in the lower half of the memory space

 

  .BooksRange :
  {
    __BOOKS_BASE = .;     #start address of the new books area
    .=ALIGN(512);
    *(.BooksRange)        #actual data matching pragma directives
    __BOOKS_END = .;
    .=ALIGN(512);
  } >> code_00020410

 

This isn't causing any errors that I can tell :smileyhappy:

 

but now I am stumped as how to get code into the BooksRange area, I tried the following but am getting

undefine macro or opcode when I insert this snippit into .asm file

 

    .BooksRange   month1: .byte 1,2,3,4,5
标签 (1)
0 项奖励
回复
1 解答
847 次查看
CrasyCat
Specialist III

Hello

 

You need to place the section BootRange that you have created in one of the memory area inside of the linker command file.

 

I assume you gave to change the definition of the section .BootRange as follows:

 

.BooksRange :  {     *(BooksRange)    . = ALIGN (0x4);} >> code_00020410 

 

 

Additionally why are you using a an org after the section command in the assembly file?

Not sure I get the point here.

 

At which address do you expect the section BootRange to be allocated?

 

CrasyCat

在原帖中查看解决方案

0 项奖励
回复
3 回复数
847 次查看
CrasyCat
Specialist III

Hello

 

As section .BooksRange  is not a predefined section you need to define it using .section directive.

 

Please look at the ColdFire_Assembler_MCU_Eclipse.pdf manual and check syntax of the .section directive.

 

CrasyCat

0 项奖励
回复
847 次查看
Kerrie
Contributor I

Thanks Crasy, you have definitly pointed me on the right path.  I no longer have compiler errors.  But I am getting this warning " BooksRange (BooksRange) is refrenced but not written check your linker command file and sure enough when I look into memory after program nothing is store in that memory location.

 

Here is the complete linker file

# Sample Linker Command File for CodeWarrior for ColdFire MCF51JE256# Memory rangesMEMORY {   code        (RX)  : ORIGIN = 0x00000414, LENGTH = 0x0001FFE8   code_00020410 (RX) : ORIGIN = 0x00020410, LENGTH = 0x0001FBF0   userram     (RWX) : ORIGIN = 0x00800000, LENGTH = 0x00008000}SECTIONS {# Heap and Stack sizes definition  ___heap_size     = 0x0400;  ___stack_size    = 0x0400;# MCF51JE256 Derivative Memory map definitions from linker command files:# ___RAM_ADDRESS, ___RAM_SIZE, ___FLASH_ADDRESS, ___FLASH_SIZE linker# symbols must be defined in the linker command file.# 32 Kbytes Internal SRAM   ___RAM_ADDRESS = 0x00800000;   ___RAM_SIZE    = 0x00008000;   # 256 KByte Internal Flash Memory   ___FLASH_ADDRESS  = 0x00000000;   ___FLASH_SIZE     = 0x00040000;  .userram        : {} > userram  .code      : {} > code  .code1     : {} > code_00020410   .text :  {    *(.text)    . = ALIGN (0x4);    *(.rodata)    . = ALIGN (0x4);    ___ROM_AT = .;    ___DATA_ROM = .; } >> code   .BooksRange :  {     *(.text)    . = ALIGN (0x4);} >> code_00020410    .usb_bdt :  {    .=ALIGN(512);    __BDT_BASE = .;    *(.usb_bdt)     __BDT_END = .;   } >> userram  .data : AT(___ROM_AT)  {    ___DATA_RAM = .;    . = ALIGN(0x4);    *(.exception)    . = ALIGN(0x4);    __exception_table_start__ = .;    EXCEPTION    __exception_table_end__ = .;    ___sinit__ = .;      STATICINIT    __START_DATA = .;    *(.data)    . = ALIGN (0x4);    __END_DATA = .;    __START_SDATA = .;    *(.sdata)    . = ALIGN (0x4);    __END_SDATA = .;    ___DATA_END = .;    __SDA_BASE = .;    . = ALIGN (0x4);  } >> userram  .bss :  {    ___BSS_START = .;    __START_SBSS = .;    *(.sbss)    . = ALIGN (0x4);    *(SCOMMON)    __END_SBSS = .;    __START_BSS = .;    *(.bss)    . = ALIGN (0x4);    *(COMMON)    __END_BSS = .;    ___BSS_END = .;    . = ALIGN(0x4);  } >> userram  .custom :  {    ___HEAP_START       = .;    ___heap_addr        = ___HEAP_START;    ___HEAP_END         = ___HEAP_START + ___heap_size;    ___SP_END             = ___HEAP_END;    ___SP_INIT          = ___SP_END + ___stack_size;    ___mem_limit        = ___HEAP_END;    ___stack_safety     = 16;    . = ALIGN (0x4);  } >> userram  __SP_INIT             = ___SP_INIT;  ___SP_AFTER_RESET     = __SP_INIT;  _romp_at = ___ROM_AT + SIZEOF(.data);  .romp : AT(_romp_at)  {    __S_romp = _romp_at;    WRITEW(___ROM_AT);    WRITEW(ADDR(.data));    WRITEW(SIZEOF(.data));    WRITEW(0);    WRITEW(0);    WRITEW(0);  }}

 

 

and here is the snippit of assembly code

 .section  BooksRange, text .org 0x0020500 testingloop: move.l #$0FF,D2  ;get current byte move.b #$03,D1 add.l D2,D1  ;D1 = D1+D2  subi.l #$01,D2  ;decrement the counter of length bne testingloop rts

 

 

0 项奖励
回复
848 次查看
CrasyCat
Specialist III

Hello

 

You need to place the section BootRange that you have created in one of the memory area inside of the linker command file.

 

I assume you gave to change the definition of the section .BootRange as follows:

 

.BooksRange :  {     *(BooksRange)    . = ALIGN (0x4);} >> code_00020410 

 

 

Additionally why are you using a an org after the section command in the assembly file?

Not sure I get the point here.

 

At which address do you expect the section BootRange to be allocated?

 

CrasyCat

0 项奖励
回复