Codewarrior DSC56800/E version 8.1.1a, build 7168 - Instant exit to Desktop

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Codewarrior DSC56800/E version 8.1.1a, build 7168 - Instant exit to Desktop

1,519 次查看
v_dave
Contributor IV

Hello All,

 

I will be submitting this as an SR request but I also wanted to post here to see if anyone has seen this before.

 

I am in the final hours of working on my project (as usual 11th hour before a tradeshow) and today my Codewarrior is crashing. 

 

Well not exactly crashing but exiting out to the desktop without any warning.  I am single-stepping through my project and out of no where Codewarrior will just disapear. 

 

This is not the normal Crash where you get a beep then a dialog box asking to send in an error report. In this instance Codewarrior just disappears.  There is no lingering process listed in Task manager, it was as if I never was running the application in the first place.

 

There is not a pattern to how\when the exit happens. The only consistant thing that happens is I am in a Break and I am either stepping through the code or trying to view a variable when Codewarrior exits.

 

Some PC Particulars:

Win XP Pro SP3

Lenovo Z60m Laptop 

Intel 1.7GhZ Pentium

2G RAM

20G HD

 

Java Runtime: Java 6 Standard - Update 11

 

Is there any additional information I need to provide?

 

Anyone experiance anything like this?  Any tips?  It has happened 10 times today so it is very frustrating.

标签 (1)
标记 (1)
0 项奖励
回复
1 回复

321 次查看
v_dave
Contributor IV
FYI - SR# 1-551117391
0 项奖励
回复