CW 6.3 (easy way) installation problem on WIN 7

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

CW 6.3 (easy way) installation problem on WIN 7

867 次查看
dpierman
Contributor II

Just installed CW 6.3 (easy method) on Win 7.  Height of window is about 1.25 inches and will not expand further.  Horizontally can expand or shrink but not vertical expansion.  Full screen makes no difference.  I have uninstalled and reinstalled but same problem.  Any ideas?

Don

标签 (1)
0 项奖励
回复
1 回复

784 次查看
vicentegomez
NXP TechSupport
NXP TechSupport

Hi

Codewarrior 6.3 was not developt for win 7, if win 7 is 64 bit, Codewarrior won't run. On system of 32 bit, it can run but this is not recommended and some function/driver does not run.

I do not know if you can move to codewarrior 10.x or 11. If not then you can use win XP if you have it.

regards

0 项奖励
回复