URGENT HELP: USB HCS08/HCS12/CFV1 Multilink - USB Port

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

URGENT HELP: USB HCS08/HCS12/CFV1 Multilink - USB Port

ソリューションへジャンプ
1,725件の閲覧回数
cremonezi
Contributor I

Hi everyone,

 

I'm using the CodeWarrior V6.2 to program a MC9RS08KA2 (2 KB Flash).

 

I'm also using a "USB Multilink" of P&E Micro (www.pemicro.com).

 

When I choose "P&E Multilink/Cyclone Pro", the window "PEMICRO Connection Manager" is open and the first field to be choosed is "Interface".

 

My problem is: if I create a new project by choosing a uC of HCS08 family, I have in this field the option: "USB HCS08/HCS12/CFV1 Multilink - USB Port". In this case, the hardware is correctly detected by the CodeWarrior.

 

However, as I really need to create a new project by choosing the uC MC9RS08KA2, I don't have anymore the option above, but "USB HCS08/HCS12/CFV1 Multilink (Rev C or Later)".

 

In this case, my USB Multilink is not detected!!!

 

Please, does anyone know what I can do to have the USB Multilink detected in this case?

 

Thank you, in advance.

Cremonezi

ラベル(1)
0 件の賞賛
返信
1 解決策
564件の閲覧回数
pgo
Senior Contributor V

Dear cremonezi,

 

I supect that your BDM does not support the RS08 chips.  These require a 12V supply for programming which is absent in the earlier versions of the P&E BDMs (before RevC?).  Is your BDM this version?

 

I suggest you check the P&E website or contact them by email to check this.

 

bye

 

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
565件の閲覧回数
pgo
Senior Contributor V

Dear cremonezi,

 

I supect that your BDM does not support the RS08 chips.  These require a 12V supply for programming which is absent in the earlier versions of the P&E BDMs (before RevC?).  Is your BDM this version?

 

I suggest you check the P&E website or contact them by email to check this.

 

bye

 

0 件の賞賛
返信
564件の閲覧回数
cremonezi
Contributor I

Hi pgo,

 

Thank you very much for your answer.

 

I've contacted the technical support from pemicro.com and you are right.

 

I have actually a USB-ML-12 Rev B, which does not support the RS08 family.

 

Best regards,

Cremonezi

 

 

0 件の賞賛
返信