S12 UNIVERSITY BOARD

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

S12 UNIVERSITY BOARD

1,434 次查看
alessandrochiru
Contributor I

I'm experiencing some trouble with S12UB (product codes: LFEBS12UB and LFEBS12UBLAB).

The stand-alone kit, provide 21 labs, to get started with 9S12 architcture.

 

The first lab (attached)  just provide the basic information to connect the debug12 module with the PC through HyperTerminal. I follow all instructions (baud=9600, 8 bits data, no parity, 1 stop bit, xon/xoff etc.), but instead of visualizing the d-bug12 bootloader, i just recive from serial port random ASCII characters.

 

I tried to change baud, connect in different ways the MODE pins, but i always get the same problem.

 

i don't have a serial port on my PC, but i emulate it wit a prolific USB-to-Serial properly configured.

 

I also don't have no idea, about what pin i have to connect with jumpers (if i have to do it).

 

Is there some specific instruction manual for S12UB?

Is it possible that data in FLASH/EEPROM memory are corrupted? how can i do to rewrite the d-bug12 program in the uC?

标签 (1)
0 项奖励
回复
1 回复

1,188 次查看
tonyp
Senior Contributor II

You will have better chances getting a reply by posting this in the 16-bit community as that's where the S12 variants are usually discussed.